Italia - Indicatore Italia

Incoterm:Reso sdoganato
Tutti i prezzi sono comprensivi di dazi e spese doganali previsti per le modalità di spedizione prescelte.

Conferma la valuta selezionata:

Euro
Spedizione gratuita per la maggior parte degli ordini superiori a 50 € (EUR)

Dollari USA
Spedizione gratuita per la maggior parte degli ordini superiori a $60 (USD)

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Monitoring Machine Operators with the OpenVINO™ Toolkit M. Tim Jones

Machine Operator Monitor Application Theme Image

According to a National Safety Council's (NSC) study, a workplace injury occurs every seven seconds. This staggering statistic equates to around 4.5 million injured workers a year. And while on-site supervisors can gauge the mood of their workers, supervisors cannot monitor workers at all times to prevent incidents. In this blog, we will explore how you can use the Machine Operator Monitor application of the Intel® OpenVINO toolkit to automatically infer a machine operator’s level of focus and mood based on video input of their facial expression. Information regarding a machine operator’s mood and level of focus can be helpful in protecting the operator from serious injury.

Machine Operator Monitor Data Pipeline

Figure 1 shows the pipeline for the Machine Operator Monitor deep-learning application. Let’s explore this pipeline and the activities that occur.

 

Operator Pose and Mood Inference Pipeline Diagram

 

Figure 1: The Operator Pose and Mood Inference Pipeline diagram illustrates how a captured image moves through the deep neural networks and the OpenVINO toolkit to identify a machine operator’s level of focus and mood. (Source: Author)

The application uses images captured by a video camera mounted on a manufacturing station. The captured image flows through a series of three deep neural networks (based on the Convolutional Neural Network or CNN). CNNs are a popular type of deep neural network that are commonly used to process images. The first CNN identifies whether a face exists in the captured frame. If the first CNN does not detect a face, then there is no need to further process the image for pose or mood. If the first CNN detects a face with a user-configurable detection threshold, the face is passed on to the next two stages. The next CNN determines whether the operator is watching the machine. The CNN does this by detecting whether the operator is facing towards the camera. The final CNN detects the operator’s facial expression. The operator must have a particular expression for a configurable amount of time for it to be considered.

Figure 2 shows an example of the completed process of these three stages of deep neural networks.

Machine Operator Monitor output screen

Figure 2: The Machine Operator Monitor screen shows an example of the output produced after this application of the OpenVINO toolkit processes the captured image. (Source: Intel)

As shown in Figure 2, the time required to detect the face as well as infer the mood and pose is around 140ms. This speed permits a fast-response time, allowing a prompt warning to the operator to minimize the chance of an accident and injury. The sample application also illustrates how the Message Queue Telemetry Transport (MQTT) protocol communicates the information to an industrial data analytics system.

Why this is Cool

The Machine Operator Monitoring application was developed with the Intel® distribution of OpenVINO and 700 lines of Go—or 500 lines of C++. This code is primarily glue code with the complex work going on in the deep neural networks pre-trained for the Machine Operator Monitor task. The first network can detect a face and check to ensure that the face rectangle is completely inside the captured frame—i.e., not a partial face. The captured image is then passed through the pose network that checks to see if the head is tilted within a 45 degree angle relative to the machine. Finally, the face image is passed into the sentiment network to identify the operator’s mood. When paired with capable hardware such as one based upon the 6th generation Intel® Core™ processor or Intel’s Neural Compute Stick 2 powered by the Intel Movidius™ X VPU, the application can deliver impressive inference speeds that enable real-time analytics.

Adapting this Example

Gaze tracking is an important new technology with many applications, but an important one today is in vehicle-driver monitoring. The 2018 Trucking Fatalities Reach Highest Level in 29 Years article by Alan Adler revealed that while motor vehicle crash deaths are declining—2 percent last year—large truck crashes rose to a 29 year high of 9 percent last year. The increase in distracted driving is one factor contributing to the rising number of trucking fatalities.

Using a deep neural network to track a driver’s head pose in real time is one way to ensure that a driver is paying attention to the road. Using information to monitor a driver’s gaze can help identify risks and ensure compliance of drivers and as a result reduce the risks that a distracted driver brings to our crowded roads.

Furthermore, you can use head pose detection in conjunction with other technologies—such as heart-rate detection, body temperature measurement, and breathing monitors—to identify drowsiness. Focusing on the eyes, monitoring blinking and eye movements could be used to detect micro-sleep—where we enter a very brief state of unconsciousness even though our eyes remain open and we appear attentive.

It’s easy to think of other applications for head pose and expression detection. Using the sample code provided, you’ll just need to use the output classification for your application, including modifying for proper head tilt.

Where to Learn More

  • You can learn more about this demonstration at Intel’s® IoT development kit GitHub.
  • The glue application was developed in the C++ and Go languages. The distribution includes the Intel® optimized face detection, head pose, and sentiment detection models for OpenVINO. You can easily experiment with this application using the Ubuntu 16.05 LTS Linux operating system, the Intel® distribution of the OpenVINO™ toolkit, and the OpenCL runtime package.
  • You can also jumpstart your development using the AIoT development kit, which includes Ubuntu, OpenVINO, Intel® Media SDK and Intel® System Studio 2018 pre-installed with an Intel® Core processor. The development kit includes tutorials to help you get up and running quickly.
  • You can also use the AAEON UP board based upon the Intel® Apollo Lake platform.


« Back


M. Tim Jones is a veteran embedded firmware architect with over 30 years of architecture and development experience.  Tim is the author of several books and many articles across the spectrum of software and firmware development.  His engineering background ranges from the development of kernels for geosynchronous spacecraft to embedded systems architecture and protocol development. 


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos